************************************************************************************

This folder contains the example codes for 16 bit Host Read and Host Write 
operation in Little Endian format for Acknowledge Mode in C for ADSP-BF52x Processors.

EZ-Kit Lite Switch Settings:
---------------------------

ADSP-BF537 EZ-Kit Lite
-----------------------

SW6 - Position 4 OFF


ADSP-BF527 EZ-Kit Lite. Host Port signals on header P13. 
--------------------------------------------------------

SW1  - Position 1, 2 off
SW5  - Position 3 off 
SW9  - Position 2, 3  off
SW11 - Position 4 off
SW13 - Position 1,2, 4 off
SW18 - Position 1,2, off
SW19 - Position 1,off
SW21 - Position 1 ON, and 2 off

Pull up of 4.7K ohm is required on HACK/ signal

Description:
------------

The required configuration either Host Write or Host Read is selected by the #define in the main.c file of the Host Project. 

For Host write operations, look for data in location 0xFF900060 and for Host Read operation fill the data at location 0xFF900060, 
so that Host reads this and places in DataIn buffer.